The following safety precautions apply to Lifting Pins, Swivel Hoist Rings, Hoist Rings, and Safety Hoist Rings. Also see the Hoist Ring section of the online or print catalog for additional precautions and installation guidelines.
Always follow all Safety Precautions, Design & Installation Requirements, and Inspection & Use Requirements
IMPORTANT! The load on each hoist ring is not simply total weight divided by the number of hoist rings. The resultant force can be significantly greater at shallow lift angles and with unevenly distributed loads. In the example below: