Each type of Carr Lane Mfg. Leveling Foot is offered in several materials and finishes, with different attrributes that apply to specific applications, such as load capacity, durabillity, and environmental factors.
Steel
Carr Lane Mfg. offers leveling feet maunfacturered from 1215 steel, carburized-hardened, zinc plated yellow chromate. This material is the most economical and wear- resistant choice for maximum load capacities.
Stainless Steel
We provide leveling feet designed with 300-series stainless steel, a material that provides excellent resistance to rust, can be sanitized, and works well in corrosive environments. Our stainless steel is DFARS and RoHS compliant.
Delrin®
White Delrin® 500 is non-marking leveling feet from Carr Lane Mfg., will not rust and can be sanitized. This material has the lowest load capacity of these materials.